9/17/2017 3:01 PM | |
Joined: 9/27/2006 Last visit: 8/9/2024 Posts: 12275 Rating:
|
Hello obasama; The Siemens S5 programming cable (connected to a PC COM port) was the 6ES5 734-1BD20, and you needed a 25 to 9-pin adapter (from any computing store) ince it was originally developped for S5 programmers (PGs) that were equiped with 25-pin serial intefaces; it is still ava It is still available, but as a spare part, which means a bit more expensive. IBH Softec also proposes a cable for S5 programming, with a USB connection to the PC; they also have a software for S5 CPUs, named S5 for Windows: https://www.ibhsoftec.com/epages/63444704.sf/en_GB/?ObjectPath=/Shops/63444704/Products/20220 Hope this helps, Daniel Chartier |
9/17/2017 4:38 PM | |
Joined: 7/15/2009 Last visit: 7/31/2024 Posts: 30 Rating:
|
Dear Mr. D Chartier, really appreciate your replay ,, i searched for this siemens product (6ES5 734-1BD20) and found it 15pin to 9pin with converter ,, and you write in your replay that it is 25pin ,, i am afraid to purchase the cable and try to connect with out any response from cpu ( will give me time out ) again thanks for interesting |
9/19/2017 4:29 PM | |
Joined: 9/27/2006 Last visit: 8/9/2024 Posts: 12275 Rating:
|
Hello samir; Two things: 1- always check for installation information from the vendor of the equipment you are buying. https://wiki.ibhsoftec.com/en/IBH_USB-S5-Adapter:SIMATIC%C2%AE_STEP%C2%AE5 You can access this page from the IBH Softec main page, Support, Wiki, USB-S5-Adapter. Check to see if you meet the minimum installation requirements and follow the step-by-step sequence as described (see the attachment below). 2- once you have purchased equipment from another vendor, you should turn to them for support, if the installation does not go to your satisfaction. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 9/19/2017 4:35:33 PM |
|
Follow us on