10/21/2015 2:50 PM | |
Joined: 10/31/2014 Last visit: 8/5/2022 Posts: 4 Rating:
|
Hi all,
I'm using TIA Portal V13 SP1, and installed the required gsd file of the RPBA and the the hardware configuration seems fine, meaning there are no errors. The next thing I did was configuring the drives so that they are controlled via communication (followed some ABB guides on how to configure them). After that I tried to use the ABB Drive Control FB from the official site http://new.abb.com/drives/connectivity/fieldbus-connectivity/profibus/profibus-dp-rpba. The problem is the block was written for Step 7 versions before TIA Portal. I managed to migrate a project with that library to a TIA Portal v13 project, but it says the blocks can't be used for S 7 1200 CPUs. On another thread I found a example by user named glinglin with the similar control block, but for the S7 1200 CPU. https://support.industry.siemens.com/tf/ww/en/posts/connect-3-abb-drives-acs550-to-an-profibus-master-in-s7-1200/75809?page=0&pageSize=10 With his example a managed to start the drive but am unable to change the reference. So, if anyone has some experience with these drives, or can help me with the mentioned example, it would be much appreciated. My goal is to send start and stop commands with the option of changing the drives reference. Thank you in advance! |
3/24/2017 12:42 PM | |
Joined: 10/31/2014 Last visit: 8/5/2022 Posts: 4 Rating:
|
Yes Ted, I managed to resolve the issue with it. |
Follow us on