2/23/2018 2:42 PM | |
Joined: 4/4/2017 Last visit: 12/1/2022 Posts: 11 Rating: (1) |
Hi, Sorry about my English and programming skills I'm a beginner :). I wanna connect user via WinCC RT v14.0 with simatic logon on windows 10 user account. For better understanding (https://www.youtube.com/watch?v=Pux9MRYnGfM and https://www.youtube.com/watch?v=6jTuyY7wvhs). I done everthing what is showed in video. I upload screens for correct understanding. Some steps what I do: 1) In WinCC RT enabled SIMATIC logon 2) Create the same group in windows 10 as is in project in WinCC 3) Create the user and add user the same group in windows as is in WinCC 4) Add user in logon role management. After this I try connect from winCC RT v14.0 to Simatic LOGON (windows account) but winCC RT do nothing. Can somebody tell me what I do wrong ? If you have some questions please write I need help with it. Thanks !
Attachmentsiemens.zip (152 Downloads) |
Last edited by: Jen_Moderator at: 2/26/2018 12:21:37 PMInserted first video. |
|
3/7/2018 4:03 PM | |
Joined: 8/3/2009 Last visit: 5/17/2024 Posts: 12970 Rating: (1651)
|
Hello STU MTF First of all if you work with Simatic Logon with WinCC Comfort/Advnaced you need a Simatic Logon remote Access countalble licence on the "Logon Server". Do you have this licence? to your Question with the RFID there is a good solution namen PM_Logon and it worked very well but its an option. It works also together with Simatic Logon. https://www.siemens.de/industrysolutions/de/en/wincc/products/pm-logon/pages/default.aspx Bye Murof |
Last edited by: Murof at: 3/7/2018 4:04:03 PMIf this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
3/8/2018 9:30 AM | |
Joined: 4/4/2017 Last visit: 12/1/2022 Posts: 11 Rating: (1) |
Hi Murof, Thank you for your answer :) I looking for in Autoamtion Licence Manager, I thnik I do not have licences for the aforementioned product. I have only licence, which you can see (JPG_1 picture). PM-Logon is good application, but If I connect my RFID reader ( MOD-RFID1356-BOX) PM_Logon does not show me card reader. I try use SIMATIC Logon but I can not changed in "Configure SIMATIC Logon" and window "Logon device" function "Logon via the following smart card reader". I found some solutions to deactiavtion terminal (https://support.industry.siemens.com/cs/document/22014042/how-do-you-log-on-via-smart-card-in-pcs-7-with-simatic-logon-?dti=0&lc=en-WW), but if i click on "deactivated terminal" after then OK and open it again, windows is in default, nothing is saved (JPG_2). Is possible log on users via another card reader like Olimex with SIMATIC Logon ? One more question. Is it possible export "user administration" from WinCC RT professional and import "user administration" to WinCC RT Advanced ? I try it, but it only creates encrypted file. Is some way where I can export "user administration" from unencrypted file ? AttachmentJPG_2.zip (147 Downloads) |
Last edited by: STU MTF at: 3/8/2018 1:44:11 PMLast edited by: STU MTF at: 3/8/2018 1:44:28 PM |
|
Follow us on