10/25/2016 10:57 AM | |
Posts: 93 Rating: (0) |
Hi cristophD, Thanks for your immediate reply. I try to install PDF 995 printer driver in simatic pc system that time THE HANDLE IS INVALID popup message appear in screen. only for checking purpose that same setup file I try to install another system (normal we are using system). that time that file open for ready to install but already install in that system but lower version.( for your information).more than two cup check same result. But My doubt is Why that popup message display in the SIMATIC PC only? what I need to be check? If any protection setting is there in SIMATIC PC, for new software installation? For better understanding, here I attached file regarding my issue. pls go through it and guide me. Advance Thanks & Regards, Suryamuni. Attachmentpdf install error.pptx (412 Downloads) |
10/26/2016 4:09 AM | |
Posts: 93 Rating: (0) |
Hi christophD, The program file(x86) is in normal we are using system. the last post we check that setup file(pdf install file) open in simatic pc and normal using pc. here I attached only the simatic pc system details and system c: file In that simatic pc only one program file is there. Thanks & Regards, Suryamuni. Attachmentsimatic pc details.pptx (348 Downloads) |
10/26/2016 10:05 AM | |
Posts: 93 Rating: (0) |
Hi christophD, Our SIMATIC PC don't have internet access. so not able to install (or) open in DOWNLOAD file. First I download that pdf995 printer drive(setup.exe) from internet, that file save to external source(like pendrive) I try in to install through pendrive same message pop uped. After that that PDF995 file save in C ----> program file that also same message pop uped. The above two trail is failed in my side. so there after, my first post asked if it's possible to install MS OFFICE and PDF PRINTER DRIVE, in SIMATIC PC. Because I don't have knowledge about SIMATIC PC. Here I attached file for open the setup.exe file through external storage(pendrive). Thanks & Regards, Suryamuni. Attachmentusing pendrive.pptx (418 Downloads) |
10/26/2016 10:50 AM | |
Posts: 93 Rating: (0) |
Hi, http://www.pdf995.com/download.html The above link I download the file, that time only one setup.exe file download. that only one setup.exe file i try to open it SIMATIC PC invalid message pop uped. So i check the NORMAL USING PC i found C ---> program file --->PDF995 ---> setup.exe. this file open time same invalid message pop uped. The above all work, if it's wrong in my side. pls guide me correct way to install the PDF PRINTER DRIVE and MS OFFICE. i need to be Installed. if any procedure is there for installing? Sorry my worst English and communication. Thanks & Regards, Suryamuni. |
Follow us on