10/11/2023 3:47 PM | |
Joined: 9/19/2023 Last visit: 10/11/2023 Posts: 3 Rating: (1) |
Hello Mauro, When i try to send something from the PLC to the HMI, nothing is happening. However, when i simulate the runtime on my pc the commands from and to the CPU are working fine, so it looks like the problem is in the HMI itself. I added the test project i am using as archived Tia V17 project. Greetz, Finn AttachmentTest project 1214DC-TP700.zip (174 Downloads) |
5/15/2024 6:57 AM | |
Joined: 4/24/2006 Last visit: 5/31/2024 Posts: 8664 Rating: (1154) |
Hello, Please have a look at the following links: Questions and answers about the security features as of TIA Portal V17 And here you can find other image files: Image Downloads for SIMATIC HMI Operator Panels: Comfort / Mobile / Basic Panels Best regards, Wizard |
Follow us on