6/8/2010 4:15 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Start - Programs - Accessoaries - System tools - System Restore SP - Service pack - In your case SP5 for Simatic Manager |
6/9/2010 3:18 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
hello, So, if you don't make any acts with hard disk, you could leave license there. But, yes it's better do not make any gambes with this. Look at How do you install, uninstall and upgrade authorizations? After ininstall of Simatic Manager, you should install it again and then eventually to update it to SP5. Best regards, Hristo Mihalev |
6/10/2010 1:58 PM | |
Posts: 107 Rating: (0) |
Hi Umencho, In the FIELD PG when I check on the item REMOVED software, there are some file with name STEP5 ( see picture S7 FILE ) Please inform me which file of S7 that I have to removed because I tried to removed "SIMATIC STEP 7 V5.4 +SP4 " then I reinstalled , but the result still the same after finish installed, I cleck on icon SIMATIC MANAGER, but the display show SIMATIC with mousein process condition but a long time, loks like HANG. I enclosed some picture that ha[ppened when I REMOVED or RE INSTALL, Please help me to solve this problem. Is there any possiblity of VIRUS on this PG ? Attachments7 install err.zip (133 Downloads) |
6/10/2010 2:33 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Step5 is different software package. About reinstall look at How can you completely uninstall STEP 7 including all the software packages? and Tips and tricks for installing and upgrading software in STEP 7 If after you still have problems, I am afraid you should recover Wondows OS. In this case make backup of all licenses there. Best regards, Hristo Mihalev |
Follow us on