11/3/2022 11:51 AM | |
Joined: 8/3/2009 Last visit: 8/2/2024 Posts: 13446 Rating: (1703)
|
Hello Mosab Soufi the Simatic Shell communication works only in the same subnet by default. But you can use one station of each subnet as Multicast Proxy in the Simatic Net terminaladapter settings. If there is a firewall between you should also use an enchrypted communication with a defined port (also in Simatic Shell Settings). Of course you have to reach the other station via ethernet (Ping OK?) Check this FAQ here you should find all information: https://support.industry.siemens.com/cs/de/en/view/109771695 Bye Murof |
Last edited by: Murof at: 11/03/2022 11:53:39If this Information really helps, you could use the Rate function |
|
12/22/2023 7:04 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8175 Rating: (169) |
New question published by AutoGen_8026329 is split to a separate thread with the subject Simatic Shell connectivity with different subnets " Server is not available". Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on