10/28/2021 7:16 PM | |
Posts: 257 Rating: (75)
|
Hello SIOS Forum Community, We keep receiving questions about the difference between SIMATIC Step 7 Basic (TIA Portal) and SIMATIC Step 7 Professional (TIA Portal). SIMATIC STEP 7 Basic (TIA Portal) Is the easy-to-use engineering system for the modular small controller SIMATIC S7-1200 and the associated peripherals. It includes S7-PLCSIM for simulating the S7-1200 CPU and SIMATIC WinCC Basic for configuring the SIMATIC Basic Panels. STEP 7 Basic is supplied with a floating licence and allows the software to be installed on any number of computers. The number of existing licences determines the number of computers on which the software can be used simultaneously. Existing STEP 7 Basic licences of previous versions can be updated to the current version with an upgrade package, STEP 7 Basic licences can be upgraded to STEP 7 Professional with the help of a Powerpack. SIMATIC Step 7 Professional (TIA Portal) Is the powerful and integrated engineering system for the current SIMATIC controllers S7-1500, S7-1200, S7-300, S7-400, WinAC and ET 200 CPU. S7-PLCSIM for simulating the S7-1500, S7-1200 CPU as well as SIMATIC WinCC Basic for configuring the Basic Panels and SINAMICS Startdrive for configuring drives are included in the scope of delivery. STEP 7 Professional is supplied with a floating licence and allows the software to be installed on any number of computers. The number of existing licences determines the number of computers on which the software can be used simultaneously. Existing STEP 7 Professional licences of previous versions can be updated to the current version with an upgrade package, STEP 7 Basic licences can be upgraded to STEP 7 Professional with the help of a power pack. Delivery release SIMATIC STEP 7 Basic/Professional V16 Another contribution in the forum deals with the Trial License Further licence types for STEP 7 Basic/Professional can be found in the Industry Mall Best regards, SIMATIC International Technical Support Hub |
10/28/2021 7:51 PM | |
Joined: 7/7/2010 Last visit: 5/2/2024 Posts: 14662 Rating: (2350)
|
I thought V17 was the current release? |
science guy |
|
This contribution was helpful to1 thankful Users |
Follow us on