7/2/2013 7:10 AM | |
Posts: 262 Rating: (45) |
HI, As the name suggests:- Simocode pro C is a varient which provieds current based protection to the motor. It can be connected to various CMM ( current measuring modules) thorugh a flat cable. It supports only DOL and RDOL feeder selection and doesn't support any expansion modules i.e. it has 4DI/ 3DO onboard + PTC connection. NO analog module, expansion DI/ DO, BTD module etc. You will get one blind operator panel for Simocode pro C and supports only profibus communication. Simocode pro V ( variable) is highly advance version Since first Simocode launched in 1986. It has all the functionality of Simocode pro C and above that supports volatge based monitoring and protection. Hence, we can have CVM ( current and voltage module) modules also used with this varient. It has 4DI/ 2DOmodule ( 2nos), 1 analog module, 1BTD module and one operator panel with display available as an expansion. ( at a time total 5nos) can be connected. It supports specific starters/ applications like DOL, Y-D, Valve, positioner, MCCB acutations etc. Recently Profinet version of simocode pro V has also launched by Siemens. AttachmentFunctions separated by device series.zip (547 Downloads) |
This contribution was helpful to1 thankful Users |
7/2/2013 7:50 AM | |
Posts: 202 Rating: (16) |
Thanks for the reply but could you please tell that for STAR DELTA connection do i need to take 3 seperate contactors? |
7/2/2013 8:04 AM | |
Posts: 262 Rating: (45) |
Yes, AttachmentY_D_Simocode.pdf (449 Downloads) |
This contribution was helpful to1 thankful Users |
5/23/2014 7:36 AM | |
Joined: 5/12/2014 Last visit: 9/9/2020 Posts: 149 Rating: (16) |
Hello, Is there any special purpose of use of SIMOCODE???
|
Follow us on