9/27/2007 7:00 PM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating:
|
Hello, easy are both! If you are familiar with SIMATIC S7 CPUs the programming of the 315T may be a bit easier, but you are limited to the functions thespecial function blocks (PLC open) offer to invoke any technological function. With the C230 you can use all SIMOTION functions, and with ST you can progam what you like. I compare it with a open field you have to cross, with SIMOTION you can gowherever you want,with a Technology CPU you havefences, that help you to cross the field, but yo can not reach any place on the field. longterm availability : both are actual products For the 31xT CPU there is a flying shears application, which may fit to your needs: http://support.automation.siemens.com/WW/view/en/21062270 |
|
|
Follow us on