4/27/2022 6:23 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Hello, Welcome to forum. Simovert MC drive which you mentioned is only inverter unit. What about DC supply? How you will connect it? Which motor do you want to run/test? Please check. |
4/27/2022 6:51 AM | |
Joined: 4/1/2020 Last visit: 3/18/2023 Posts: 4 Rating: (0) |
Yes, I justmentionedinverter unit. I have been supplied 510V DC for Simovert and I have connected U2 V2 W2 with 3 phase asynchronous motor, and I also supply 24 VDC pin 1,2 of X9. Everything is ok , now you show me to test motor running. Thanks |
4/27/2022 7:22 AM | |
Joined: 4/1/2020 Last visit: 3/18/2023 Posts: 4 Rating: (0) |
|
4/28/2022 6:57 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
You can not connect asynchronous motor to MC drive. It only supports 1FK6, 1FT6, 1PH7, 1PL6, 1PH4 motors. You can only test inverter without connecting motor. Please refer attached sheet for parameter setting. Hope this helps. |
Follow us on