11/26/2017 10:59 PM | |
Joined: 3/9/2016 Last visit: 2/25/2023 Posts: 7 Rating: (0) |
Friends, is it possible to simulate Profinet communications between an S7 300 and an S7 400? I have read and tried many ways of communication between these 2 PLCs, but I have not managed to get any good results. I have done simulations using SFB12 "BSEND" and SFB13 "BRCV" or SFB8 "USEND" and SFB9 "URCV" or SFB14 "GET" and SFB15 "PUT" I have tried these 3 ways and I have not had any good results, I want to do this simulated work, because my network is big, and I must have everything ready when I have space to download the program, but I am worried that communication does not work in this way. My only alternative that I have left, is that the PLC SIM does not support this type of communication to be able to simulate it will this be possible? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/27/2017 1:21:34 PMNew subject after splitting |
|
11/27/2017 1:55 PM | |
Joined: 3/9/2016 Last visit: 2/25/2023 Posts: 7 Rating: (0) |
Hello I'm using step7 v5.5 sp4 Rev.Lev K5.5.4.0, and PLC SIM V5.4.SP5 + Upd2 Rev.5.4.5.2 |
11/27/2017 2:50 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (820) |
Hello, look here: TCP PLCSim Issue If you mean real Profinet I/O I think this isn't working in this PLCSim, but maybe other guys gives better info. |
With best regards... |
|
11/27/2017 3:11 PM | |
Joined: 7/9/2015 Last visit: 9/25/2024 Posts: 3945 Rating: (586) |
Hi, if you want to simulate over CP it´s not possible. Please check the following FAQ: What is the difference between S7-PLCSIM and a "real" automation system?There you will find SFB/SFC which will work with integrated interface of PlC with PLCSim. Regards, Towome |
|
|
This contribution was helpful to3 thankful Users |
11/27/2017 3:49 PM | |
Joined: 3/9/2016 Last visit: 2/25/2023 Posts: 7 Rating: (0) |
I'm going to try it thank you very much |
This contribution was helpful to1 thankful Users |
Follow us on