11/5/2019 8:15 PM | |
Joined: 6/8/2017 Last visit: 4/10/2024 Posts: 2 Rating: (0) |
Hello, I have v15.1 loaded and I can select the 6 inch basic panel with v12 firmware and download to a 6 inch v12 firmware hmi but when i try to simulate this hmi it does not work. If i change device to a 7 inch ktp and simulate, it works fine. Any Solutions for the Sim and 6 inch hmi with v12 firmware? Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/06/2019 07:42:47New subject after splitting |
|
11/5/2019 9:22 PM | |
Joined: 12/18/2014 Last visit: 5/4/2024 Posts: 32956 Rating: (4073) |
Make screenshot(s) of the error Messages and upload as Zip file, if you more then one screenshot. |
11/6/2019 7:58 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
hi, have you check PG/PC Settings in windows control panel? Regards Christoph |
Follow us on