2/23/2019 8:42 AM | |
Joined: 3/3/2016 Last visit: 12/26/2023 Posts: 140 Rating: (0) |
Sir! I have Sinamic G120 PM240-2 ,CU320-2PN and CPU1214C .Now which software to connect this two device via profinet. |
2/23/2019 9:33 AM | |
Posts: 1283 Rating: (105) |
STEP 7(TIA PORTAL) you can use this for PROFINET and also for programming S7-1200 devices. Configuration Topic Maybe this thread can help you undertsnad a bit more. You may need to configure the driver using the starter software and then import GSDML file to TIA and integrate with s7-1200 |
Last edited by: Jay. at: 2/23/2019 9:37:44 AM |
|
2/23/2019 10:36 AM | |
Joined: 3/3/2016 Last visit: 12/26/2023 Posts: 140 Rating: (0) |
IF HAVE ANY SAMPLE PROJECT |
2/23/2019 10:39 AM | |
Joined: 3/3/2016 Last visit: 12/26/2023 Posts: 140 Rating: (0) |
THE MOTOR USE IN TENSION CONTROL |
3/6/2019 8:07 AM | |
Joined: 3/3/2016 Last visit: 12/26/2023 Posts: 140 Rating: (0) |
HI! In logo cpu any analog output is there? |
Follow us on