12/31/2018 9:45 AM | |
Joined: 2/7/2015 Last visit: 2/10/2024 Posts: 33 Rating:
|
HelloGanesh Karthik, for your first question : When optimization become complete the measuring status switch to No measure again . After that you should copy RAM to ROM and save file to PG(Uploaded) . For second question: If your motor work above base speed you have to determine the minimum of current of field because of field weakening! Regards |
12/31/2018 3:28 PM | |
Joined: 2/7/2015 Last visit: 2/10/2024 Posts: 33 Rating:
|
If you not working in field weakening you should put max. and min. current of field same.Here is 21.7A |
Follow us on