12/5/2020 5:40 AM | |
Posts: 22 Rating: (0) |
Hello there, I have sinamics drive S120 double motor module version 1P-6SL3120-2TE21-0AA3. I want to communicate with Starter version 4.1. 1)What will be steps for the same ? 2) How to ensure communication is properly established 3) what will be type, version, Bus addr. of given drive version. Thank You, Pranjal Gajjar ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/07/2020 10:27:24New subject after splitting |
|
12/5/2020 6:40 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello Pranjal, Please do not post in old topic & do not create multiple posts for your issue. Simply post your query in correct product conference & wait. Forum memebrs will definately reply to your post. Meanwhile you can search related topics by enetering texts in search box which you can find at right top side. After enetering related text in search button, you will find related information like, product note, download, application example, FAQ, manual etc. etc. Now about your query, part number you mentioned is of motor module. User can not establish direct communication with motor module. Check which CU i.e. is CU310 or CU320 is connected which controls S120 drive. Further more, check if this CU is on any network like profibus or ethernet etc. etc. STARTER is commissioning tool with which you can commission, back up paramaters of Sinamics drive. With ethernet cable, PG/PC can be interface with CU unit ethernet port & via STARTER data can be accessed. Please refer Application exampleSINAMICS S120 Getting Started with the STARTER Commissioning Tool which will help you to understand how to set up communication & access drive data. HTH |
This contribution was helpful to2 thankful Users |
12/5/2020 8:45 AM | |
Posts: 22 Rating: (0) |
Please find the attachment. |
12/5/2020 9:37 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
What is the application? How drive is controlled? Is any CUA or PLC or HMI is connected? |
12/5/2020 10:07 AM | |
Posts: 22 Rating: (0) |
Yes, sinumerik 802D S L provided. |
12/5/2020 10:10 AM | |
Posts: 22 Rating: (0) |
Sinumerik 802D SL is available |
12/5/2020 12:17 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
You should have post this query in SINUMERIK CNC automation systems product conference. Please refer Multiple alarms in 802d controller for more detail information. |
This contribution was helpful to1 thankful Users |
12/7/2020 3:51 PM | |
Joined: 8/21/2014 Last visit: 9/19/2024 Posts: 1024 Rating: (14) |
As you followed the advice and posted the question again in a the SINUMERIK CNC automation systems conference this topice is closed. The second thread with the subject [Communication with Sinamics S120 by Starter 4.1 ] is published within the conference [SINUMERIK CNC automation system]. Best regards The Helping Hand
|
My Forum is the place to personalize your profile, |
|
Follow us on