2/25/2019 8:21 PM | |
Joined: 4/2/2016 Last visit: 7/13/2022 Posts: 413 Rating:
|
it's about this SINAMICS S120 Synchronism Applications with DCB Extension ??? if yes, then in the section Which licenses / software packages are necessary....talking about CU320, not CU310!!! Runtime License: For using the required DCB Extension libraries „GMC“ and „math_extended“ a DCB Extension Runtime License per Control Unit CU320-2 is needed. MLFB DCB Extension Runtime License: 6SL3077-0AA00-0AB0 (1 License per device – not per axis!) (Activation of Trial License Mode for maximum 3 Trial License Periodes with 300 hours each is possible) Could you tell us in more detail what you want to do? for example, why you don't want to use one CU320 and two PM? and make inside CU320 master-slave? Note: really can connect one profinet encoder to two CU310PN? it will work without PLC? |
Last edited by: _oleksandr_ at: 2/25/2019 8:35:30 PMLast edited by: _oleksandr_ at: 2/25/2019 8:35:42 PMLast edited by: _oleksandr_ at: 2/25/2019 8:37:10 PMLast edited by: _oleksandr_ at: 2/25/2019 8:37:43 PMLast edited by: _oleksandr_ at: 2/25/2019 9:02:04 PMLast edited by: _oleksandr_ at: 2/25/2019 9:03:06 PMLast edited by: Jen_Moderator at: 2/26/2019 11:15:15 AMOptimized link. |
|
Follow us on