12/13/2019 12:21 PM | |
Joined: 3/2/2015 Last visit: 2/3/2023 Posts: 60 Rating:
|
Hi Everyone, I am working on a fatigue test application. We are using S120 CU320-2PN to control a PM240-2/1FT7105 motor with absolute encoder. Required motion profile is sinusoidal, simple up/down motion for the coupled vertical axis. I am generating a sinusoidal waveform of required amplitude and frequency from a CFC in drive. The output of this CFC is a sine curve which I connected with p1155 of drive. Control mode is speed control with encoder (p1300=21). The problem that we are facing is that after around 2000-3000 oscillations we notice a visible offset from center point of target position. Ideally the axis should move with fixed high/low displacement positions centered around the target position. But instead the high/low points continue to shift in the positive direction. However the displacement remains fixed. Any idea what could be the causing this? Attached are trace screenshots for reference. Regards, Anas Attachmenttrc.docx (14 Downloads) |
12/13/2019 12:33 PM | |
Joined: 4/23/2010 Last visit: 1/29/2023 Posts: 7962 Rating:
|
Have you tried with p1300 = 21 velocity control with encoder! |
12/13/2019 12:42 PM | |
Joined: 3/2/2015 Last visit: 2/3/2023 Posts: 60 Rating:
|
Yes sir, it is mentioned above in post |
Follow us on