7/25/2016 4:32 PM | |
Joined: 4/18/2016 Last visit: 3/15/2022 Posts: 7 Rating: (30) |
Hello Guys, I am holding an Issue. I have configured drive output for 4-20mA. I have receiving mA up to the TB, but when I connect to the ET200SP Analog input module, it gives its full count of 32767(20mA). I have configured the module for Two wire 4-20mA also I have checked the connections. It feels strange. Kindly help me to get out of this issue.
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 7/25/2016 4:48:46 PMNew subject after splitting |
|
Follow us on