9/25/2021 8:41 PM | |
Joined: 11/9/2020 Last visit: 7/19/2022 Posts: 4 Rating: (0) |
Hello Everyone, I'm getting the error that was in the FAQ but was not clear to me how to solve the issue as presented in the explanation. Also for the project, I'm doing right now, I'm not using a brake thus, I didn't attach anything to the cable. There is nothing coupled to the motor shaft at this moment. Solution: >In the moment of pole position identification at first starting, if the motor is the statue of running (eg: external force), the pole position identification will be failed cause. Please reidentify the pole position of the 1FL6 TTL motor under the immobile status of the motor.
Regards |
Follow us on