4/17/2018 12:10 AM | |
Joined: 4/2/2016 Last visit: 7/13/2022 Posts: 413 Rating:
|
S7 1200 (HSC)+ encoders TTL 5V? I have a positioning system based on S7-1200 and Sinamics V90 + 1FL6061-1AC61-0AB1, two axes, control - Pulse / Direction Interface. similarly as in the example SINAMICS V: Controlled Positioning of a V90 with S7‑1200 via the Pulse/Direction Interface, with HMI (Set 7) for control Pulse / Direction Interface I use 2 fast digital output (for each axis), SB 1222 DC 200 kHz 6ES7222-1BD30-0XB0. the example does not use position feedback, but I would like to use signals from the motor encoder, Sinamics V90 has an encoder output (TTL 5V), 6 outputs (A+,A-; B+,B-; Z+,Z-), And I would like to read it, S7-1200 have High-Speed Counters (HSC) x6 pcs., to each HSC can connect 3 digital inputs (eg., A+, B+, Z+), for two axes I need 2xHSC (6 digital inputs), the problem is that encoder output from Sinamics V90 TTL (5V DC), and HSC S7-1200 HTL 24V DC, we have different voltages, of course I could use an additional card 5V DC (eg. SB 1223 DC/DC 200 kHz 6ES7223-3AD30-0XB0), but I'm already using SB for fast digital output SB 1222 DC 200 kHz. What can you advise me? What kind of equipment (converter TTL/HTL) required? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/17/2018 9:09:42 AMNew subject after splitting |
|
This contribution was helpful to
1 thankful Users |
4/17/2018 9:11 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
Closed cause question posted twice.
|
My Forum is the place to personalize your profile, |
|
Follow us on