4/28/2006 3:26 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hallo, i did not have some "Know-how" about S7 200, but did you check the settings from the PPI cable? Did you have a nother project which you can test the performance? I found some infos about kommunication to a S7 200 and a RT => http://support.automation.siemens.com/WW/view/en/16650850 (For PrTool, but it should be same for WinCC flexible) => http://support.automation.siemens.com/WW/view/en/14188898 => http://support.automation.siemens.com/WW/view/en/16532946 => http://support.automation.siemens.com/WW/view/en/16810372 It is a big project? If yes, what are, if you reduce the Project (tags, which communicated to the flexible RT) greetings, |
Follow us on