11/18/2021 4:38 PM | |
Joined: 5/16/2016 Last visit: 5/21/2024 Posts: 42 Rating: (7) |
I am posting to help anybody out there who is experience similar issues. My facility is running PCS7 9.0 SP1 with SIMATIC Logon V1.6, with two OS servers and 15 clients. I was contacted by operations that the HMIs were very slow. Working with a production lead we walked up to a WinCC entered user information into the SIMATIC prompt. It took about 15 minutes before the user was logged on. Once the user was logged on the WinCC client functioned normally. I contacted Siemens support and they stated that most likely culprit was slow authentication and to look into the AD (Active Directory) server. I spoke to the IT team and found out we have two redundant ADs. I executed the following command on the WinCC client "echo %logonserver" in cmd prompt and it returned that the secondary domain controller was the logon server. The IT team turned off the second domain controller. I then rebooted the client and executed the echo command, the return showed that the primary domain controller was active. The logon response time did not improve. The IT team reset the netlogon services on the primary controller. I then logged onto a WinCC client via SIMATIC logon and the authentication took a less than 5 seconds. In short, if you WinCC clients are slow to authenticate when using SIMTAC logon start with AD controller and work down from there. A helpful post: Computer is slow to authenticate - Active Directory, DNS issue? | 4sysops |
Why you troubleshoot? |
|
Follow us on