Industry Online Support
Technical Forum
1/30/2014 11:40 AM | |
Joined: 8/25/2005 Last visit: 11/28/2023 Posts: 1161 Rating:
|
Hello Francisco Oliveira, of course the GSD-File is available. Please have a look here: PROFIBUS GSD files : SIMATIC The DP-Slave which would be conected is your CPU. So you need the GSD-File of the CPU. The Moduls are configurable. Just select the corresponding one within the configuration of the Slave. Good luck Sabine |
This contribution was helpful to
1 thankful Users |
1/31/2014 4:30 PM | |
Joined: 8/19/2013 Last visit: 2/14/2019 Posts: 148 Rating:
|
Hello Francisco, as i understand you in the right way you want to connect the listed modules to the third party F-CPU the only way to use the failsafe modules is on the one hand in the central rack of the S7-300F CPU or on the other hand in a decentral station ET200M. These links may help you PROFIBUS ET200M http://support.automation.siemens.com/WW/view/de/113498?Datakey=58100448 PROFINET ET200M http://support.automation.siemens.com/WW/view/de/25057900?Datakey=58101095 They are really hidden ;) Regardsand good luck |
This contribution was helpful to
1 thankful Users |
2/13/2014 9:00 AM | |
Posts: 341 Rating:
|
new question is splittet to ET200M with safe I/O modules connect to non-Siemens safety CPU. |
Follow us on