12/11/2013 4:52 PM | |
Joined: 4/29/2010 Last visit: 8/12/2024 Posts: 1557 Rating: (161)
|
Hello Homeroid_BL, there is a application wich can help you in this case a lot i think: User-defined Web Sites for HMI Operator Units At this application you can find at chapter 3.3.2 the information: Access to subfolders If you are using your WinCC flexible confi guration to structure the “subfolder” tags, you have to indicate this with the tag declaration on the HTML page ( Link ). The respective folders are then separated with a “\\”. Example: The “Tag_01” tag is located in the “Machine_01/Tag_01” folder HTML code: <BODY > .... Tag value: <MWSL><!--write(GetVar(" Machine_01\\ Tag_01")); --></MWSL> .... </BODY> With best regards |
12/11/2013 9:21 PM | |
Posts: 211 Rating: (6) |
That's it! Variables accessed. Thanks, Sandman! |
Follow us on