9/25/2016 3:26 AM | |
Joined: 3/28/2010 Last visit: 12/24/2024 Posts: 1099 Rating: (216) |
It is impossible to answer your question with the information you've provided. Some transmitters are 4-20mA with no digital communications, others are HART, others Profibus PA or Foundation Fieldbus. TH300 is HART and needs a HART modem with either PDM (with EDD file) or Pactware software (with DTM file) TH400 is either Profibus PA or Foundation Fieldbus. PDM would need the appropriate GSD file and whatever hardware is needed for PDM to talk PA. Siemens lists a DTM file (Pactware) but I have no clue what hardware is used for Pactware Profibus PA. |
Follow us on