4/1/2016 4:26 PM | |
Posts: 5 Rating: (0) |
Hi all, I have the same problem: hardware installed but not shown in the list. I found it in non-standard profile but when I open a project the CPU doesn't appear in the hardware configuration. Step7 V5.5+SP4, Release K5.5.4.0 How can I solve? Thanks, Massimo ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/4/2016 12:21:15 PMNew subject after splitting Last edited by: MassimoMilluzzo at: 5/27/2016 9:14:27 AM |
|
4/4/2016 12:33 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
Hello, this llok like a defective installation of the HW Catalog. Please try to reinstall SP4 and show if the error was fixed. The SP4 setup you can download here: https://support.industry.siemens.com/cs/de/en/view/93842624
Christoph |
Last edited by: ChristophD at: 4/4/2016 12:38:12 PM |
|
This contribution was helpful to1 thankful Users |
4/6/2016 4:03 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835)
|
Hello, First, Please give us MLFB (Part Number) of your CPU |
Ayman Elotaify |
|
4/6/2016 4:11 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
please look on the screenshot. The marked folder in the screen contains the MLFB, and the Folder is not expandable -> data missing! Christoph |
4/6/2016 5:16 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835)
|
Hello, Please try to download and install its gsd file from this link. It may be corrupted or may be somebody removed it by mistake |
Ayman Elotaify |
|
4/6/2016 5:30 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
WTF? The GSD object is not displayed in Simatic manager like a PLC from the HW Catalog! Regards Christoph |
Follow us on