3/20/2024 10:55 AM | |
Joined: 2/17/2020 Last visit: 4/26/2024 Posts: 993 Rating: (169) |
Hi, Do you have SIMATIC NET installed and licensed on the Unified PC? if you communicate with more than ten controllers with the RT Unified, as is your case (13), SIMATIC NET and the IE S7 license are required. Please see: SIMATIC NET Licences for WinCC Unified PC Runtime I would also recommend you avoid selecting the <Auto> option of the network card for the access point of the PG/PC Interface tool. |
A rating will be well appreciated. |
|
This contribution was helpful to2 thankful Users |
3/20/2024 7:53 PM | |
Joined: 1/20/2014 Last visit: 4/22/2024 Posts: 2 Rating: (0) |
Thank you. You are probably right. But interest that the runtime not show any information about missing licenses. |
Follow us on