1/31/2008 8:25 PM | |
Posts: 2661 Rating:
|
The INI file stores the entries in the initial mask. ??????ST.S5D is the actual program file from which youtransfer blocks (OB's/FB's/DB's etc.) to the PLC. And??????Z0.SEQ is the symbols file. The error you are getting is because the location of program file stored in the INI file does not exist. You can safely ignore this, type in the proper program file and symbol file names and you are good to go. A good place to start learning S5 is to download the manuals (for example 95U) from the support site: http://support.automation.siemens.com/WW/view/en/17220769 Good luck! |
2/13/2008 2:56 AM | |
Posts: 5 Rating:
|
why do these file say f drive when they are in c drive? |
2/13/2008 3:03 AM | |
Posts: 5 Rating:
|
I did that 3 in 1 test and I am getting this error also is there a way of fixing the drive location above? |
Last edited by: dan65bigdog at: 13.02.2008 03:07 |
|
2/13/2008 5:42 PM | |
Posts: 2661 Rating:
|
Which version of STEP 5 are you using? SIMATIC STEP 5 V7.2 |
Follow us on