9/6/2006 11:32 PM | |
Joined: 1/7/2006 Last visit: 7/3/2023 Posts: 2705 Rating:
|
Hi CarpeDiem, To work with STEP5 and STL you may read the next handbook: SIMATIC STEP 5 V7.2 [:P] Further are there operationslist / reference guideswith all the commands, such like S5-115U Programmable Controller CPU 941/942/943/944 Reference Guide and also in the handbooks of the sevaeral S5 PLCs there is a explination of the commands S5-115U Programmable Controller. [8)] If you need it for another type of CPU/PLC system then search for that by typing by search 100U, 95U, 115U, 135U or155U and look only for the handbooks. [;)] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
This contribution was helpful to
1 thankful Users |
9/7/2006 4:15 PM | |
Posts: 2 Rating:
|
I have some pdf manuals, but didnt find what I was looking for. I`ll study links thay you gave me. Thank you for the fast answer. |
9/13/2006 2:44 PM | |
Posts: 38 Rating:
|
Hi CarpeDiem, Pleasedownload manual of S5 90U/95U from the link given below and refer Chapter 8 Step 5 Operations. Same way you may refer to the manual of the CPU you want to program. http://support.automation.siemens.com/WW/view/en/1091648 Regards, PRK |
Last edited by: O_Moderator at: 9/16/2010 3:14 PMlink edited |
|
Follow us on