6/15/2016 1:20 PM | |
Joined: 7/9/2015 Last visit: 4/26/2024 Posts: 3814 Rating: (554) |
Hi, I try to answer some questions... 1. Do i have to use an additional software together with STEP7 & LabView? -> in S7 you should have all FCs, FBs to use with esisting Simatic Hardware; in LV I don´t know... 2. Can i use serial interfaces like:RS232 & RS485 to do this? and how? Serial interfaces are no problem, check FAQ: How and in which S7 stations can you use serial communication modules? 3. Can i use Ethernet interface to do this? and how? Yes, in S7 you can i.E. communicate with integrated PN-Interface of your PLC or you use a CP, FCs and FBs are also available in libraries. Regards, Towome |
|
|
This contribution was helpful to1 thankful Users |
Follow us on