Industry Online Support
Technical Forum
7/8/2011 1:46 PM | |
Joined: 3/21/2006 Last visit: 7/12/2023 Posts: 10221 Rating:
|
Hello, Take a look there http://support.automation.siemens.com/WW/view/en/36184919 Best regards, Hristo Mihalev |
7/8/2011 10:35 PM | |
Posts: 8946 Rating:
|
No, NOT. never. niemals nie nicht. |
7/9/2011 6:45 AM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 1/28/2009 Last visit: 9/25/2023 Posts: 6822 Rating:
|
Also check this: Which version of STEP 7 is compatible with which version of Microsoft Windows operating system? Configuration Notes Definitively the only operating systems that are released are those which are explicitly listed in the readme file. The table below shows you as of which version of STEP 7 there is compatibility with which Microsoft Windows operating system.
2) As from STEP 7 V5.1 incl. SP2 you require SP1 for MS Windows 2000. 3) No support planned from MS Windows XP Home. 4) MS Windows 95b or MS Windows 95 OSR2 required for OEM versions. 5) MS Windows 98 SE (Second Edition) required. 6) SP6a for MS Windows NT 4.0 required. 7) At least SP1 for MS Windows 2000 required. 8) MS Windows 2000 Professional at least SP3 required. 9) MS Windows XP Professional SP1 recommended. Not released for MS Windows XP Professional SP2. 10) MS Windows XP Professional SP1 or SP1a required. For MS Windows XP Professional SP2 you require STEP 7 V5.3 SP2. Not released under MS Windows XP SP2c. 11) STEP 7 V5.3 incl. SP2 is not enabled for use in MS Windows Server 2003 incl. SP1. 12) MS Windows Server 2003 as workstation computer, STEP 7 V5.3 SP2 required 13) MS Windows 2000 Professional SP4 required. Not released for STEP 7 V5.4 SP4. 14) MS Windows Server 2003 standard edition and MS Windows Server 2003 SP1 standard edition as workstation computer. For STEP 7 V5.4 SP4 Windows Server 2003 SP2 is required. 15) MS Windows XP Professional SP1 (or SP1a) or SP2 required. For MS Windows XP Professional SP3 you require STEP 7 V5.3 SP2. Not released under MS Windows XP SP2c. 16) As of STEP 7 V5.4 SP3. STEP 7 is not released for MS Windows Vista Home Basic and Premium. 17) Windows XP Professional SP2 or SP3. 18) Windows Server 2003 SP2 / R2 SP2 standard edition as workstation computer. 19) Windows 7 32 Bit Ultimate Professional and Enterprise (standard installation). However, the Windows XP mode in Windows 7 is not released. Not released for Windows 7 + SP1. |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Follow us on