6/1/2011 9:06 AM | |
Posts: 272 Rating: (4) |
Hi All, Can you please tell me that if i install the Stuxnet PAtch in my infected PC wether it will effect my existing backups ??? |
6/1/2011 9:08 AM | |
Posts: 8946 Rating: (999) |
yes it will. Have a look hered: http://support.automation.siemens.com/WW/view/en/43876783 |
6/1/2011 10:25 AM | |
Posts: 212 Rating: (12) |
hi, IBN, the patch installed for removing stuxnet threat will affect the project backup????? |
6/2/2011 9:05 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi all Thank you IBN-Service, Thats a good tip to find out the affected files. Have fun... |
Jazz |
|
6/2/2011 9:58 AM | |
Posts: 212 Rating: (12) |
add more to IBN-Service, - up-to-date virus scanner as per released compatibility matrix only. and up-to-date Virus definition regularly. I know few users who do it every other day.. virus definitions arereadily available on every antivirus site for related package. - switch of "automatic update" feature of the Windows administartion - check compatibility and effect of security pages on Siemens Service Support Website before installing. - some users now have shifted to use PS2 mouse instead of USB mouse to protect the system.as same USB port can be used to insert removable media. Iread that now security of Control systems standard ISA 99 shall now address the issues like warms,viruses and threats refer the link http://www.isa.org/InTechTemplate.cfm?Section=Standards1&template=/ContentManagement/ContentDisplay.cfm&ContentID=85577 |
This contribution was helpful to1 thankful Users |
6/2/2011 10:06 AM | |
Posts: 8946 Rating: (999) |
Become SAVE not become CRAZY.... |
This contribution was helpful to1 thankful Users |
Follow us on