4/17/2023 6:06 AM | |
Joined: 1/21/2013 Last visit: 5/4/2024 Posts: 2742 Rating: (444)
|
Hi DaveB14, Congratulations on your first post. More information is needed to answer your question. However, it is better to contact Siemens Technical Consulting as they take responsibility for their answers. You can use the contact database to find the contact for your location. You should consider the following:
Kind regards |
4/17/2023 8:43 AM | |
Joined: 1/21/2013 Last visit: 5/4/2024 Posts: 2742 Rating: (444)
|
Hi DaveB14, If you focus on the SCALANCE X Industrial Ethernet Switches, your options start with the SCALANCE XC-200 or XP-200 series, as these Layer 2 switches also support NAT, which is a Layer 3 functionality. For full Layer 3 functionality, you need to use the X-400 or X-500 series. However, if OPC UA is required, the use of NAT can be critical, see "What are the causes when connection to an OPC UA server fails?". So I will still recommend to ask for help at Siemens Technical Consulting. Kind regards |
Follow us on