9/11/2024 8:09 AM | |
Joined: 1/21/2013 Last visit: 12/20/2024 Posts: 3396 Rating: (530)
|
Hi Rivas, The rendering of SVG graphics in WinCC Unified Engineering System as well as on the WinCC Unified Panel is done by the same code (I think since V18) and should therefore be identical. In your case, the appearance in the browser is different, but this is mostly a browser issue. Using the style related attributes instead of CSS styling should solve your problem. Please try the attached file. Kind regards AttachmentRivas_Kant_601_V10.zip (149 Downloads) |
9/11/2024 7:43 PM | |
Joined: 1/21/2013 Last visit: 12/20/2024 Posts: 3396 Rating: (530)
|
Hi Rivas, To optimize SVG files I use SVGOMG. It offers many features and one of them is 'Style to attribute'. Kind regards |
Follow us on