Industry Online Support
Technical Forum
1/11/2015 9:37 PM | |
Posts: 7 Rating: (0) |
OK. I am running out of things to try. A while back, the project was in a bad way via a failed compile of some sort... Not sure what happened as I was not on site when the issue occured, but the long and short of it is since then we have had lots of issues. I feel fairly confident that blocks from the F systems library were accidently added to an AS without the same library but the other engineer has not said that happened so I am not sure? The most recent issue is the inability to add blocks to an existing CFC. This includes copy / paste or inserting from the library. The block being added that causes the issue is not always the same. A few days ago it was PA_AO. I cleaned up runtime groups by deleting unused groups and moving blocks to a fewer number of groups. I have completed ENTIRE AS compiles since then as well so I am not sure exactly what helped out. Today it seems to be ANY block. The other day it wout allow blocks to be added and then a few blocks later it will stop allowing it. I can sometimes compile and restore the ability to add blocks. The most recent time it has not corrected the issue it seems. I also tried a Save As with reorganization, but I had another error come up when I did that. The error (I wish I had taken a screenshot) was presented when I went to download to the AS (changes only). The site is a 24/7 facility and it will not be allowed to put the AS in STOP. Any ideas would be greatly appreciated. Screenshots attached are of the initial error screen when the block is dropped in the CFC and the associated details when the OK button is pressed. ANY ASSISTANCE is greatly appreciated!
Attachmentsystemerror.zip (162 Downloads) |
1/12/2015 4:43 AM | |
Joined: 11/26/2011 Last visit: 6/29/2023 Posts: 508 Rating: (22) |
I read about this problem before in the forum. its related to F blocks only. It was problem with the antivirus (microsoft security essential) after uninstall this error 1739:10 gone. if you have av program uninstall it and try. And one morelink..
|
This contribution was helpful to2 thankful Users |
Follow us on