12/16/2006 3:47 PM | |
Posts: 1 Rating:
|
I am using Step 7 v5.3 sp3 (fresh install). I have a project that we have used previously on a CPU 317-2 PN/DP, we received a new PLC of the same type, but it will not let me download the application. Below is the given fault message, I can not find how to change the PLC type to anything but a v5.2 (from the currently selected 5.3). From my reading this is a 'relatively new' v5.3.4 I think, but I do not know how to make my Step 7 recognize it. System data download to station SIMATIC 300 Station is not being executed because the target module differs from the configured module CPU 317-2 PN/DP (rack 0, slot 2). -> Order number: 6ES7 317-2EJ10-0AB0 (offline), 6ES7 317-2EK13-0AB0 (online) Thank you for any help.. link |
Last edited by: WStocker at: 12/16/2006 5:24 PMhttps://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=23183356&objAction=csOpen&caller=view&lang=en&siteid=cseus&aktprim=0&extranet=standard Last edited by: WStocker at: 12/16/2006 5:22 PMLast edited by: WStocker at: 12/16/2006 5:22 PM::Update:: Finally found document below, which enabled the selection of the new Order Number to replace the PLC with. Since original hw_update2 site does not exist, finding the update was not easy. (The below link lead to Hardware Update [Support] Packages) https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.cs |
|
12/17/2006 2:43 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi W, You may need a Hardware Support Package, see the link Hardware Support Packages (HSPs) You may implement the new CPU in de hardware projecting, please read the pdf thats also in this ID. The newer CPU haves more memory and is further the same. If the software is written for the older CPU, you may get the MMC and place that directly into the new CPU. You can load the software also, the message will come that there is a difference but thats only a message. Better is it to update the HW-projecting with a HSP and programm the newer CPU... |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on