5/4/2023 8:30 PM | |
Joined: 6/11/2019 Last visit: 7/13/2024 Posts: 2205 Rating: (99) |
Hello jtm2605, In my experience, operators who already have difficulties with a potentiometer are unable to master the complexity of entering values. Wouldn't it be better to limit the maximum value of the potentiometer and only make this upper value available for a specific group of users ? You can see a simple limitation of the potentiometer in the appendix, where everything over 50% is cut off. But you could also use the entire adjustment range of the potentiometer and take the limited value as the end stops. greeting Ella_68 (translated with Google) AttachmentProgrammplan2.zip (342 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on