5/20/2016 1:55 PM | |
Posts: 2 Rating:
|
Thanks for your quick response. I've made screens to show in a clearer way how I made the communication, because I think my post wasn't explicit enough (it's my first). Each capture have a number as name, I'll use them to develop step by step : 1 : I put telegram 390 in my PLC data types with the sinamics telegram library. 2 : I create a DB block, which contains the telegram 390. 3 : I add in my device config the telegram 390, like I had to do with telegram 111 (this last is working perfectly), but in "DO Control Unit", not in "Servo" 4 : I note the hardware identifier for the next step. 5 : I create a network, the same as I did for telegram 111 for my X-axis. 6 : I can see that I receive information from my CU, but from now I don't know what to do, I tried to force to "1" Inputs/outputs on Starter and it doesn't change in Tia Portal, and reciprocally. Starter 1 : all I did in Starter was to put "Telegram 390" instead of "Free", like you can see. I hope that I've been more clear now, and that you can help me to make it work. Thanks in advance ! :) AttachmentScreens tel390.zip (311 Downloads) |
Follow us on