8/6/2020 9:45 AM | |
Joined: 2/6/2019 Last visit: 4/16/2024 Posts: 33 Rating: (0) |
Hello, I have this task. Connect to a PLC 1200 with Teleservice. Hardware: 1200 + DI+DO+ Cp 1242-7 Already this configuration is connected with another same 4 configuration with telecontrol ( TCSB - TELECONTROL SERVER BASIC V3.1.0.3) Now I want to connect remote to a station, and I follow the steps from ( https://support.industry.siemens.com/cs/ww/en/view/56720905 ) with no succes. I guess i don't configure IP correctly. So maybe someone can help me. I will atach all the print with information from my configuration ( PLC station + TCSB) |
Last edited by: Jen_Moderator at: 08/06/2020 11:11:14Optimized link. |
|
8/6/2020 10:12 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello CezarAdrian, there is also a FAQ in the internet and I hope this could be meaningful for you. How do you configure cyclic data exchange between an S7-1200 CPU (with CP 1242-7) and the telecontrol server? With best regards |
Follow us on