9/8/2016 6:32 PM | |
Joined: 3/14/2016 Last visit: 8/11/2023 Posts: 162 Rating: (45) |
What language are you using? STL? You can use pointers to address to the temp area. You can also use the AT at the 32 bools structure you have and use symbolic. You just have to be careful to which function temp area you're moving to. I'm currently facing a problem to move variables to the temp area when I call more than 2 functions. The problem, as well as some explanations about how to use pointers, can be found here. |
"Engineers like to solve problems. If there are no problems handily available, they will create their own problems." (Scott Adams) |
|
9/9/2016 9:11 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi AGEnes, with the newer CPUs you can overlapping tags with the AT-keyword. have a look to this FAQ: How do you program the overlapping of tags with the keyword "AT" in the STEP 7 (TIA Portal)?hope this helps, regards, |
FCK WAR! |
|
9/9/2016 11:48 AM | |
Posts: 5225 Rating: (1185)
|
Hi, You already have a good solution - the AT overlay. May I suggest another solution Greetings. |
Follow us on