Industry Online Support
Technical Forum
8/2/2012 2:20 PM | |
Posts: 33 Rating: (0) |
Hello, good morning. Every time I download the program to plc 1200, I always compile 2 FCs in particular. when I asked permission to download the program shows: TEST AND COMMISSIONING FUNCTIONS ACTIVED What does that mean? I have had many problems with a previous program, and I suspect it has something to do with this function _________________________________________________________________________ Hola, Buenos días. Cada vez que bajo programa, noto que siempre muestra que compila 2 FCs en particular y cuando me pide la autorización para bajar el programa aparece lo siguiente: FUNCION TIS ACTIVA Que significa eso? He tenido muchos problemas con un programa anterior, y sospecho que tiene algo que ver con esa funcion _________________________________________________________________________ THANKS FOR READ IT! AttachmentImágenes.zip (183 Downloads) |
8/3/2012 8:11 PM | |
Posts: 33 Rating: (0) |
Está con el pack de servicio 2 y con la actualizacion 3... _________________________________________________ It is with service pack 2 and the update 3 ... |
4/10/2014 3:36 PM | |
Posts: 6 Rating: (1) |
I too faced this problem. After clicking on the PLC from Local modules tab and then downloading the hardware solved it. |
Follow us on