9/9/2019 12:25 PM | |
Joined: 7/7/2016 Last visit: 8/14/2024 Posts: 3 Rating:
|
I also have an M5 PG with STEP5 and got the same error as you when I try to select the "Prommer Type" (see attachment 1 & 2). Is the program you used called "STEP 5 EPROM Programming V1.2"? (Found on: https://support.industry.siemens.com/cs/document/109744421/in-step-5-why-do-you-get-the-error-message-hardware-error-when-you-want-to-transfer-your-program-to-an-eprom-?dti=0&lc=en-GB) When I attempt to use this software I still get errors?? See attachment 3. It states "EPROM driver registers an error, Error no.: 784, USB prommer locked / not connected". In the box with the M5 I didnt get a USB Prommer, I got S5 Prog Adapter 6ES7798-0CA00-0XA0. I have attempted to restart my M5 multiple times with this device connected however unable to resolve... Any guidance would be appreciated. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/10/2019 05:56:58New subject after splitting |
|
This contribution was helpful to
1 thankful Users |
9/9/2019 12:38 PM | |
Joined: 7/7/2016 Last visit: 8/14/2024 Posts: 3 Rating:
|
|
9/9/2019 12:38 PM | |
Joined: 7/7/2016 Last visit: 8/14/2024 Posts: 3 Rating:
|
|
Follow us on