10/26/2021 10:52 AM | |
Joined: 9/22/2017 Last visit: 12/14/2023 Posts: 7 Rating: (0) |
Hi! I want to use the "System Information" channel and the "Printer status" variable. The default address is: F = 15.1, Name In the "WinCC Communication" manual I read that "The server name must be entered in the ‘Printer’ field" What does that mean exactly? What should I enter instead of "Name" in the "Address" field? ------------------------------------------------------------------------------------------ |
Last edited by: Piotr58 at: 10/26/2021 10:54:23Last edited by: The Helping Hand at: 10/26/2021 12:36:34New subject after splitting |
|
10/26/2021 2:52 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello Piotr58, if you have a networkprinter, you need to set the printserver and printername
Georg Berghof |
Last edited by: bg2492 at: 10/26/2021 15:09:37PS: If this post did really help you, you may use the Rate-button |
|
10/26/2021 3:02 PM | |
Joined: 9/22/2017 Last visit: 12/14/2023 Posts: 7 Rating: (0) |
@Georg - Thank you very much |
Follow us on