4/13/2022 6:21 PM | |
Joined: 12/7/2009 Last visit: 5/13/2024 Posts: 33 Rating: (9) |
Hi @Vijayant & @0_Einstein I do have a similar issue. I have a S120 CU320-2PN V5.2 & S7-1214C DC/DC/DC CPU. Configuration using the GSDML was a piece of cake till here. But I have a BLM (20kW, Infeed Module), A single motor module with 1PH80871SNxxx Motor. Hardware configuration under distributed I/O is possible using the hardware from GSD. Compilation also doesn't result in any error. But once I downloaded the correctly configured compiled configuration, TIA could not recognise the entire S120 group device (Device not reachable). Surprisingly if i remove control unit & infeed module from the S120 device under distributed I/O & just configured DO Servo & added Standard Telegram 1 or 2 or 3 (same thing configured for axis in Starter), there are no compilation errors & device will be error free from TIA online. But unfortunately it is not an axis. I just need speed & direction control for my connected asynchronous 1PH8 (induction) motor. This function is not possible to configure in the selected Telegram. If i go for a free telegram, i am landing up with an error saying the size of the selected Telegram is not sufficient for the configured functions. Version of TIA didn't really matter. I tried with V14, V14.1, V15, V15.1, V16 & V17 (All fully featured 21 days trial installation). All with latest updates & HSP update. For S7-1500 CPUs it works smoothly even if i configure directly from Hardware catalogue or even from GSD. Problem is only with S7-1200. Local official support couldn't comission the same & the BOM was technically verified by Local Siemens prior to ordering. How to run this setup!!!??? ------------------------------------------------------------------------------------------ |
Last edited by: Bharath Sharma at: 04/13/2022 18:29:10Last edited by: Jen_Moderator at: 04/20/2022 14:17:28New subject after splitting |
|
4/21/2022 9:50 AM | |
Joined: 10/11/2006 Last visit: 5/13/2024 Posts: 5837 Rating: (790)
|
Hello Bharath Sharma, I assume that you use STARTER or SCOUT, do you? Have you already tried to use the official script to generate the GSD? Please also make sure that the Profinet name and IP address are correct. |
With best regards, |
|
Follow us on