3/17/2014 9:37 AM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating: (43) |
hey, there are some possibilities for you... as you are saying you want to read a more than a few bytes, perhaps you have to use sth like the open communication --> use the ag_send/ag_recv functions to communicate with your third party device. if you really just want to communicate over the process image, then you can (i-slave, e.g.) define the accessible data. then you have to configure afterwards only address and speed. Perhaps have a look at the compendium and/or at the programming manual of step 7 for some hints regarding the I-Slave. |
Best Regards, |
|
Follow us on