6/21/2022 3:55 PM | |
Joined: 6/18/2022 Last visit: 8/2/2022 Posts: 8 Rating: (0) |
Hello Techno_Taru Sorry for late response and hope you are doing fine. attached document is the one I followed to make a project for communication over TCP/IP from Profinet of Controller. Please tell how can I make a project with available libraries of PCS V9.1 to make this communication between to AS possible. Thanks in advance. because file was too big I split it into two files. AttachmentModbus TCPIP PCS 7 driver blocks pages 1 to 30.pdf (228 Downloads) |
6/21/2022 3:57 PM | |
Joined: 6/18/2022 Last visit: 8/2/2022 Posts: 8 Rating: (0) |
second file AttachmentModbus TCPIP PCS 7 driver blocks pages from 30-68.pdf (197 Downloads) |
6/22/2022 7:53 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi SF1360, the Modbus TCP/IP PCS 7 driver blocks library is not a default library of PCS 7. To get the library and the license you have to contact function.blocks.industry@siemens.com. After the installation of the Modbus TCP/IP library you can find the library under <installation directory>SIEMENS\STEP7\S7libs by default is that C:\Program Files (x86)\SIEMENS\STEP7\S7libs. For more information have a look at the manual Modbus TCP/IP. With regards |
This contribution was helpful to2 thankful Users |
Follow us on