5/30/2014 6:52 PM | |
Posts: 165 Rating: (19) |
Hello , Recently I am using TIA Portal V11 SP2 . Unfortunatly I am suffering very badly due to unexpected crashes while programming. Recent days i am not able to open Menu&Toolbar configuration ... I have created one Thread but cant solve problem..... After that I have created support request to siemens.. I Got a very accurate reply Dear Sir , Please install Update 5 for WinCC V11 SP2 The same can be downloaded from:- http://support.automation.siemens.com/WW/view/en/58112582 Now After Updating TIA V11 sp2 to Update-5 ..many of my problems solved. Menu and Toolbar configuration is working ok. Software stablity increases a bit. Hence , As per my experience If you are Using TIA V11 SP2 you should update your software Download Available in above link. But If it is possible to upgrade TIA V11 to V12 or V13 then you should go for that first.
|
This contribution was helpful to4 thankful Users |
5/30/2014 7:02 PM |
|
Posts: 784 Rating: (52) |
Nice thread. |
5/30/2014 7:06 PM |
|
Posts: 165 Rating: (19) |
Thanks..
|
5/30/2014 7:14 PM |
|
Posts: 24 Rating: (0) |
Nice Tipp for TIA V11 |
5/30/2014 7:31 PM | |
Posts: 165 Rating: (19) |
DearIBN-Service, We must move on to TIA V12 or V13 if we don't want to suffer more. Because TIA V12 & V13 I found more stable version than TIA V11. But rite now I am working on a TIA V11 project so no option other than upgrading the software.
|
5/31/2014 7:11 AM | |
Joined: 1/28/2012 Last visit: 7/23/2024 Posts: 519 Rating: (83) |
[quote user="PDGANGANI"]Hello , Recently I am using TIA Portal V11 SP2 . Unfortunatly I am suffering very badly due to unexpected crashes while programming. Recent days i am not able to open Menu&Toolbar configuration ... I have created one Thread but cant solve problem..... After that I have created support request to siemens.. I Got a very accurate reply Dear Sir , Please install Update 5 for WinCC V11 SP2 The same can be downloaded from:- http://support.automation.siemens.com/WW/view/en/58112582 Now After Updating TIA V11 sp2 to Update-5 ..many of my problems solved. Menu and Toolbar configuration is working ok. Software stablity increases a bit. Hence , As per my experience If you are Using TIA V11 SP2 you should update your software Download Available in above link. But If it is possible to upgrade TIA V11 to V12 or V13 then you should go for that first.
Thanks for sharing your experience. It might help other to resolve issue regarding TIA V11. .
|
Regards, |
|
This contribution was helpful to1 thankful Users |
5/31/2014 9:48 PM |
|
Posts: 559 Rating: (87) |
Good Job. |
6/1/2014 6:57 AM |
|
Posts: 165 Rating: (19) |
Thank You..SolutionFinder
|