3/1/2016 11:14 PM | |
Posts: 3 Rating: (0) |
hello everyone!! recently I've updated my TIA family to v13 SP1.I heard that S7-1200 simulation had some repairs in last version but there is no difference.....I can't get online or download my program to virtual device. at first I open PLC SIM and create a new project for S7-1200 then I compile my hardware with no problem. in ''extended download to device'' window as you see in the following picture,I had a compatible device in target subnet.after selecting that device and pressing load button,the ''load result'' windows appears as shown in the picture and I have an error while loading and downloading.I don't know where the problem is. I should say that I test the same action with S7-1500 and the other families without any problem. in my control panel, the ''set pc/pg interface'' access point of the application is ''PLCSIM S71200/S7-1500'' and assigned as ''PLCSIM S71200/S7-1500.TCPIP.1'' who can tell me the proper steps for getting online or downloading?where is the problem? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/2/2016 9:37:00 AMNew subject after splitting |
|
3/2/2016 9:38 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
Closed cause question posted twice. The second thread with the subject Tia V13 SP1, can't get online or download my program to virtual device is published within the conference STEP 7 (TIA Portal). Best regards Min_Moderator |
Last edited by: Min_Moderator at: 3/2/2016 9:39:34 AM |
|
Follow us on