12/17/2020 10:30 AM | |
Joined: 3/11/2019 Last visit: 5/6/2024 Posts: 1399 Rating: (248) |
Dear dan.v. please find two screenshots attached. For example, if in V13 a CP (or any other device) with security features was configured, it was necessary to activate the user management. To activate the user management, it was necessary to enter a username and password. If you want to upgrade the project to a newer version, you will have to enter the user/password that was previously entered for configuration of the security features. In project without user management, the entry "Global security settings" in project navigation is missing. Maybe this helps STEP 7 Professional V13.1 - Managing rightsRegards sancruz |
Last edited by: sancruz at: 12/17/2020 10:33:45Feedback appreciated, please rate |
|
This contribution was helpful to1 thankful Users |
12/18/2020 11:25 AM | |
Joined: 7/1/2014 Last visit: 3/18/2024 Posts: 230 Rating: (24) |
I checked and I have that "security" voice, but no hardware like CP that could have enabled it... I dont understand why its there! And again I have not user+password, everything is on full access too... I would expect to have the same request when I try to do V13 to V14, but that works... the problem is there only if I try to upgrade from V13 to V15 or V14 to V15! ???? I will now check the link you shared too
|
Follow us on